Real Time

Signal IO

1. Marker

2. Aux Port General Settings

Marker 1

State

Marker 3

Data Polarity

Marker 4

 

3. Multiplexed Mode Setup

4. Dedicated Mode Setup

First Address

Aux Port Pin

Second Address

Baud Rate

5. Aux Pin/Bit Select

 

Transmit Power Contol Source

 

1. Marker

Marker 1

Choice: Even Second | Super Frame (80ms) | Radio Frame (20ms) | Power Control Group (1.25ms) | Sync Channel Frame (25.666...ms) | Delayed Even Second Clock (2s) | System Reset

Sets the data source of Marker 1 for the output signal.

[:SOURce]"RADio:CDMA2000[:BBG]:MKR1 ESECond|SFRame|RFRame|TPControl|SCFrame|DESecond|SRESet

[:SOURce]"RADio:CDMA2000[:BBG]:MKR1?

ESECond

Even Second (2s)

SFRame

Super Frame (80ms)

RFRame

Radio Frame (20ms)

TPControl

Transmite Power Control Frame (1.25ms)

SCFrame

Sync Channel Frame (25.666...ms)

DESecond

Delayed Even Second

SRESet

System Reset

Marker 3

Choice: Even Second | Super Frame (80ms) | Radio Frame (20ms) | Power Control Group (1.25ms) | Sync Channel Frame (25.6ms) | Delayed Even Second Clock (2s) | System Reset

Sets the data source of Marker 3 for the output signal.

[:SOURce]"RADio:CDMA2000[:BBG]:MKR ESECond|SFRame|RFRame|TPControl|SCFrame|DESecond|SRESet

[:SOURce]"RADio:CDMA2000[:BBG]:MKR3?

Marker 4

Choice: Even Second | Super Frame (80ms) | Radio Frame (20ms) | Power Control Group (1.25ms) | Sync Channel Frame (25.6ms) | Delayed Even Second Clock (2s) | System Reset

Sets the data source of Marker 4 for the output signal.

[:SOURce]"RADio:CDMA2000[:BBG]:MKR4 ESECond|SFRame|RFRame|TPControl|SCFrame|DESecond|SRESet

[:SOURce]"RADio:CDMA2000[:BBG]:MKR4?

2. Aux Port General Settings

State

When disabled, all the data sent to the AUX port will be ignored by this I/Q channel.

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:[:STATe] ON | OFF | 0 | 1

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:[:STATe]?

Data Polarity

Choice: Negative| Positive

Default: Negative

Determines whether the AUX input data will be inverted or not. If "Negative" is selected, the AUX input data will be inverted.

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:DATA:POLarilty POSitive | NEGative

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:DATA:POLarilty?

3. Multiplexed Mode Setup

In Multiplexed Mode, 4 pins in AUX port will be used as addresses, the other 12 AUX pins are used as data.

First Address

Choices: Unassigned | Group 1 | Group 2 | Group 3 | Group 4 | Group 5 | Group 6 | Group 7 | Group 8 | Group 9 | Group 10 | Group 11 | Group 12 | Group 13 | Group 14 | Group 15

Default:Group 1

Coupling: grayed out unless Operating Mode is set to Multiplexed Mode

Selects an additional address (different from broadcast address) to receive AUX I/O data.

The data comes with this address value will be transmitted to this I/Q channel.

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:MULTiplexed:ADDR1 GROUP1|GROUP2|GROUP3|GROUP4 | GROUP5|GROUP6|GROUP7|GROUP8 | GROUP9|GROUP10|GROUP11|GROUP12 | GROUP13|GROUP14|GROUP15

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:MULTiplexed:ADDR1?

Second Address

Choices: Unassigned | Group 1 | Group 2 | Group 3 | Group 4 | Group 5 | Group 6 | Group 7 | Group 8 | Group 9 | Group 10 | Group 11 | Group 12 | Group 13 | Group 14 | Group 15

Default:Group 2

Coupling: grayed out unless Operating Mode is set to Multiplexed Mode

Selects another additional address (different from broadcast address) to receive AUX I/O data. The data comes with this address value will be transmitted to this I/Q channel.

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:MULTiplexed:ADDR2 GROUP1|GROUP2|GROUP3|GROUP4 | GROUP5|GROUP6|GROUP7|GROUP8 | GROUP9|GROUP10|GROUP11|GROUP12 | GROUP13|GROUP14|GROUP15

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:MULTiplexed:ADDR2?

4. Dedicated Mode Setup

To activate this mode, in Instrument Node, click on Operating Modein Aux IO Global Controls and select Multiplexed.

In Dedicated Mode, also called Serial Mode, for each application, only one Aux pin is used as AUX input.

Aux Port Pin

Choices: AUX0 | AUX1 | AUX2 | AUX3 | AUX4 | AUX5 | AUX6 | AUX7 | AUX8 | AUX9 | AUX10 | AUX11

Default: AUX0

Selects a serial pin from which the application channel wants to receive AUX port data (dedicated mode only).

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:DEDIcated:PIN NONe | AUX0| AUX1| AUX2| AUX3| AUX4| AUX5| AUX6| AUX7| AUX8 | AUX9| AUX10| AUX11

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:DEDIcated:PIN?

Baud Rate

Range: 9600 | 14400 | 19200 | 38400 | 57600 | 115200 | 230400 | 460800 symbols per second

Default: 230400

Coupling: grayed out unless Operating Mode is set to Dedicated Mode

Specifies how fast the serial data is transmitted (in symbol per second), which can be set in remote GUI or using the SCPI commands shown as follows:

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:DEDIcated:DATa:RATe 9600|14400|19200|38400|57600|115200|230400|460800

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:DEDIcated:DATa:RATe?

5. Aux Pin/Bit Select

Transmit Power Control Source

Operating Mode = Multiplexed Mode

Choices: AUX0 | AUX1 | AUX2 | AUX3 | AUX4 | AUX5 | AUX6 | AUX7 | AUX8 | AUX9 | AUX10 | AUX11

Default: AUX0

Operating Mode =Dedicated Mode

Choices: BIT0 | BIT1 | BIT2 | BIT3 | BIT4 | BIT5 | BIT6 | BIT7

Default: BIT0

Select the AUX port or bit as transport power control source. This is same meaning as External Data Input Port in Tx Power Control node.

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:TPC AUX0 | AUX1 | AUX2 | AUX3 | AUX4 | AUX5 | AUX6 | AUX7 | AUX8 | AUX9 | AUX10 | AUX11 | BIT0 | BIT1 |BIT2 |BIT3 |BIT4 |BIT5 |BIT6 |BIT7

[:SOURce]"RADio:CDMA2000[:BBG]:AUX:TPC?